Technical FAQs

Ask a Question

Can 25-38kV HVL/cc switchgear be sold as front access only?

It is best to have rear access, but in most cases it can be done without having it. C phase cannot be reached from the front and B phase if difficult. It is somewhat easy to climb into the cubicle in all cases except Application A incoming units with an instrument compartment. Those are easily accessible from the top, except for outdoor, which should not have top entry any way. Important: When climbing into the cubicle one must be careful where they step. Do not step on the switch housing, only on the supports at the edges of the cubicle.


CTA-ID : 2018460
Was this helpful?
What can we do to improve the information ?