Technical FAQs

Ask a Question

Why do the UPdt and UPdH functions not show up as an option for Fr1 but are available under Fr2 code in the CtL menu when LAC is set for level 2 or 3?

To set up the unit for + speed / - speed as either UPdt, via LI (logic inputs), or UPdH, via the up and down arrow keys, use the Fr2 code under the CtL menu.  
The programming manual indicates that this can also be done in Fr1, but that is incorrect.

Reviewed 6/2011

CTA-ID : 2018114
Was this helpful?
What can we do to improve the information ?