Technical FAQs

Ask a Question

Does the QU816D400SL have a main breaker?

Yes, it contains a factory installed QDL22200 main breaker feeding the 8-16 interior, which contains Feed-Thru lugs and with provisions for a second field installed Service Disconnect up to 200amp maximum.


CTA-ID : 2018846
Was this helpful?
What can we do to improve the information ?