Technical FAQs

Ask a Question

What are the magnetic trip settings for a MAL26600?

The AC magnetic settings are:
low = 3000
high = 6000
(UL magnetic trip setting tolerances are + or - 25%(low) and + or - 20%(High) from nominal values shown)


CTA-ID : 2018841
Was this helpful?
What can we do to improve the information ?