Technical FAQs

Ask a Question

Can additional gutter space be added to NQOD Panels?

Yes, this is something that needs to be done on Product Selector. See page 4-9 in the supplemental digest 173.

Revised 6/24/04


CTA-ID : 2018816
Was this helpful?
What can we do to improve the information ?