Technical FAQs

Ask a Question

Is an Ethernet card an option of the Econo-Flex drive?

No. This is not standard for the Econoflex drive. It would have to be a special modification. Contact SquareD field office.
However, the Ethernet card is an available standard option on the 58M product line. This is Mod D09 on the 58M and must also have option F07 for control.


CTA-ID : 2018451
Was this helpful?
What can we do to improve the information ?