Technical FAQs

Ask a Question

What size of lugs are used in the PBQ4660G/PBQ3660G 600A plug-in unit?

There are two of the 3/0 - 600 kcmil lugs per phase and neutral. There is one of the #6 - 300 kcmil lug for ground.

CTA-ID : 2018212
Was this helpful?
What can we do to improve the information ?