Technical FAQs

Ask a Question

Customer has two EZM326N. Needs to replace handle assembly.

Will need to replace the complete molded case switch with p/n MHL360006M if used a molded case switch. If the old knife blade type the Handle assembly is p/n 40512-172-50 SEL

CTA-ID : 2018442
Was this helpful?
What can we do to improve the information ?