Technical FAQs

Ask a Question

What is the combination suffix code for the 1021 shunt trip and the 2100 alarm contact on a KA breaker?

Use the 2200 suffix for FA, KA, LA, MA, NA type breakers. Use 2253 on PA and PE type breakers.
See Digest or use product selector for Powerpact catalog numbers


CTA-ID : 2018274
Was this helpful?
What can we do to improve the information ?