Technical FAQs

Ask a Question

Why does the ATV58 drive sometimes stop running though the drive state still shows ``rdY`` when using with an N2 card (sometimes there is SCF or OPF fault.)?

Check the revision of the control board and the N2 card.
The drive should be V5.1 or greater and the N2 card should be V1.1 IE03 or greater.

CTA-ID : 2018267
Was this helpful?
What can we do to improve the information ?