Technical FAQs

Ask a Question

Can the ATV31 unit accept a PWM or pulse train signal as speed reference command?

No.
The analog inputs accept 0-10 VDC, 4-20 mA or 0-20 mA signals.
Digital inputs (Logic inputs LI1 to LI6) can be used for preset speeds or jog speeds.
It is also possible to use the keypad or serial communications (Modbus RS-485) to control the speed.


CTA-ID : 2018113
Was this helpful?
What can we do to improve the information ?