Technical FAQs

Ask a Question

What are the repair parts for a H326NDS Series E4 Heavy Duty Safety Switch?

Previous design Repair Parts

Product Line:
Heavy Duty Safety Switches


The parts listed here are the only field replaceable parts.
Line base assembly - 4055218550SEL (3-required and arc suppressor assembly is not included)
Load base assembly - 4055218750SEL (3-required)
Arc suppressor assembly - 4051204501 (3-required)
Lug assembly - 4405044601 (2 required per base assembly)
Neutral assembly - H600SN
Line base phase insulator - 4051201401 (2 required)
Load base phase insulator - 4055219101 (2-required)
Line & load base mounting screws - 4020600901 (2 required per base assembly)
Handle assembly - 4051219150SEL
Vault handle - 4051219450SEL
Handle knob kit - 4401142750 (the black & red knob at the end of the handle)
Neutral bonding strap - 4028325350SEL

CTA-ID : 2018761
Was this helpful?
What can we do to improve the information ?