Technical FAQs

Ask a Question

What are the AIC ratings of a KAL, 600Vac max. thermal-magnetic circuit breaker?

They are as follows:
at 240Vac = 42kA
at 480Vac = 25kA
at 600Vac = 22kA


CTA-ID : 2018752
Was this helpful?
What can we do to improve the information ?