Technical FAQs

Ask a Question

Is ground fault protection available on Class 2730 CTC assemblies for units of 800A and less?

Ground fault protection is available only on units of 1000A and 1200A.


CTA-ID : 2018745
Was this helpful?
What can we do to improve the information ?