Technical FAQs

Ask a Question

Is the keyed switch on the 9001 Security Stations spring return to center from both sides?

Yes these control stations are spring return to center from both sides.


CTA-ID : 2018737
Was this helpful?
What can we do to improve the information ?