Technical FAQs

Ask a Question

Can the External RFI Input Filters (VW3A58401, VW3A58402, VW3A58403, VW3A58404, VW3A58405, VW3A58406, VW3A58407 or VW3A58408) listed in the catalog for the ATV58 TRX unit be used on the Econo-Flex packages?

The mounting will not be the same as on an open type ATV58. However, it can be mounted externally to the enclosure.
Note: This inquiry and response is not to be confused with the EMC filters that can be installed on these drives.
The EMC filters are to meet requirements of EMC Directive Level A.
To achieve Level B compliance, install an external RFI filter.

CTA-ID : 2018300
Was this helpful?
What can we do to improve the information ?