Technical FAQs

Ask a Question

How do you order a NEMA Size 3, 4, or 5 starter with 2 normally open and 2 normally closed auxiliary contacts factory installed ?

Add form X22 to the starter catalog number.

CTA-ID : 2018421
Was this helpful?
What can we do to improve the information ?