Technical FAQs

Ask a Question

What is the function for the security key on a XCSE7313?

A tubular high security key operated lock allows the force opening of the guard in an emegency situation. When the tubular high security key is turned to the unlock position, the acutating key is unlocked and is free to be removed from the switch.


CTA-ID : 2035457
Was this helpful?
What can we do to improve the information ?