Technical FAQs

Ask a Question

How many wires can be terminated in each hole of a panelboard neutral bar?

You may use one neutral wire per hole on the neutral and two on the ground lug.

Revised 5/25/04

CTA-ID : 2018092
Was this helpful?
What can we do to improve the information ?