Technical FAQs

Ask a Question

What is the length of the cat whisker on a 9007C54K?

The dimension from the center line of the top mounting holes of the switch body to the tip of the cat wisker is 5.50`` or 140mm


CTA-ID : 2018090
Was this helpful?
What can we do to improve the information ?