Technical FAQs

Ask a Question

Do we have a flip cover that does not hold button in depressed position for the 9001 KR4 KR24 KR5 KR25 mushroom head operators?

Issue:
Do we have a flip cover that does not hold button in depressed position for the 9001 KR4 KR24 KR5 KR25 mushroom head operators?
Product Line:
30mm Push Buttons                       
Environment:
9001 type K/SK Padlock attachments
Cause:
Application is calling for a flip cover on the operator that does not hold the button depressed.
Resolution:
We do not offer a flip cover for the mushroom operators that does not hold the operator in depressed position.
 
Was this helpful?
What can we do to improve the information ?