Technical FAQs

Ask a Question

What is the dimension from the endwall of the box to the lugs of the main circuit breaker on Class 2730 CTC units rated 1200A?

The dimension is 16.21 inches.


CTA-ID : 2019161
Was this helpful?
What can we do to improve the information ?