Technical FAQs

Ask a Question

What is the dimension from the endwall of the box to the lugs of the main circuit breaker on Class 2730 CTC units rated 400A-1000A?

The dimension is 18.94 inches.


CTA-ID : 2019160
Was this helpful?
What can we do to improve the information ?