Technical FAQs

Ask a Question

Can the M9PAF be used on all C60N breakers and supplementary protectors, regardless of the number of poles?

The M9PAF can be used on 1, 2 , 3 or 4 pole C60N supplementary protectors, both UL1077 and UL489 versions.


CTA-ID : 2018052
Was this helpful?
What can we do to improve the information ?