Technical FAQs

Ask a Question

Does Square D offer a EZM 400amp Branch device that contains two 200amp tenant breakers instead of only one 400amp tenant breaker?

Issue:
Current EZM Design

Product Line:
EZM Metering

Environment:
Branch Devices

Cause:
Metering Application

Resolution:
No. Square D does not offer a 400amp EZM Branch device that contains two 200amp tenant breakers. ALL the EZM, 400amp branch devices available, contain ONLY a single 400amp tenant breaker. 


CTA-ID : 2018196
Was this helpful?
What can we do to improve the information ?