Technical FAQs

Ask a Question

Can the handles rated for 200A - 400A be used with the GS1JU3 100A switch?

Yes, it can. The only difference in these handles is the length of the grip. For example, the GS1AH430 handle has a 5`` grip whereas the standard GS1AH410 handle has a 3`` grip.


CTA-ID : 2018191
Was this helpful?
What can we do to improve the information ?