Technical FAQs

Ask a Question

Does the molded case switch used in the QO200TR, enclosure have a `HACR` rating?

Issue:
Product Design Features

Product Line:
Enclosed Molded Case Switches 

Environment:
Device Ratings

Cause:
Application

Resolution
No, the QO200 Molded case switch used in the QO200TR does NOT provide overcurrent protection, therefore does NOT have 'HACR' ratings. Because ONLY overcurrent protection devices, like a circuit breaker, have 'HACR' ratings.



CTA-ID : 2035379
Was this helpful?
What can we do to improve the information ?