Technical FAQs

Ask a Question

Can a QO112M100 Convertible load center be ordered with a 50A main breaker, instead of a 100A one?

Issue:
Product Design features

Product Line:
QO Load Centers

Environment:
Main breaker

Cause:
Application

Resolution:
Yes. the catalog number QO112M10050 cand be ordered from the factory.


CTA-ID : 2018398
Was this helpful?
What can we do to improve the information ?