Technical FAQs

Ask a Question

What is the minimum height required above plug-in busway for mounting FA/FH circuit breaker plug-in units?

Per the table on page 62 in catalog 5600CT9101, 10`` is required from the centerline of the bus duct to the ceiling.


CTA-ID : 2018189
Was this helpful?
What can we do to improve the information ?