Technical FAQs

Ask a Question

Can a 250 amp frame KA breaker with an electric motor operator be used in an I-Line panel?

The side mount KAM01 electrical operator can be used in an I-Line panel, HCM or larger. The KAM01 will require an additional 4.5`` of mounting space. NOTE: Electrical operators cannot be used on vertically mounted main breakers.

Revised 7/7/04


CTA-ID : 2019066
Was this helpful?
What can we do to improve the information ?