Technical FAQs

Ask a Question

Are the RL... Line Reactors listed in our pricing guide a 3% or a 5% reactors?

From the MTE Corporation`s home page (Our Source) the line reactors for 480v Three Phase and 208/230 V Three Phase are 5%. The line reactors specified for the 208/230 V Rated Single Phase are 3%.

CTA-ID : 2019056
Was this helpful?
What can we do to improve the information ?