Technical FAQs

Ask a Question

Are the Class 9065 Type SS410 and Type SS420 provided lugs?

Yes, these overload are for separate mount and are supplied with line side and load side lugs.


CTA-ID : 2019052
Was this helpful?
What can we do to improve the information ?