Technical FAQs

Ask a Question

What is the part number of the special software for ATV58 drives for Kal Kan?

S313 is the code to designate the special software for Mars, M & M, Kal Kan, for the Altivar 58 drive.
The drive part number ends in S313U in place of the U. For example, an ATV58HD16N4XZU drive would be ATV58HD16N4XZS313U to include the special software.
This software pre-assigns LI4 for freewheel stop. With this software LI4 cannot be changed. Instruction Bulletin 30072-450-49 gives further information.
It is also possible to get the special S313 control board. The control board part number is VX4A581S313.

CTA-ID : 2018967
Was this helpful?
What can we do to improve the information ?