Technical FAQs

Ask a Question

Is the part number VW3A58352U for Lonworks option card available for the ATV58?

The correct product is the LonWorks to Modbus Module part number VW3A58312PU.
The part number that was listed in the 172 Digest is not correct.

CTA-ID : 2012324
Was this helpful?
What can we do to improve the information ?