Technical FAQs

Ask a Question

Does the ATV31 have a display value that can be customer defined and scaled to correspond to machine speed, process speed or motor speed?

Yes.
The display code SPd1 or SPd2 or SPd3 is for the output value in customer units.  These code values depend on the SdS parameter.  See the VVDED303042US or VVDED303042NA Programming manual for details.  Factory setting is SPd3.
SdS is the scale factor for the display parameter.  It is used to scale a value (such as motor speed) in proportion to the output frequency rFr.

Reviewed 6/2011


CTA-ID : 2018693
Was this helpful?
What can we do to improve the information ?