Technical FAQs

Ask a Question

Are either of the generator panels, catalog numbers QO48M30DSGP or QO48M60DSGP, available in a NEMA 3R enclosure?

Issue:
Product Design Features

Product Line:
QO Load centers

Environment:
Enclosure Rating

Cause:
Application

Resolution:

No. These catalog numbers are available in NEMA 1 enclosures ONLY. Consider a standard Main Lugs NEMA 3R load center with a field installed Manual Transfer Equipment Kit.


CTA-ID : 2017509
Was this helpful?
What can we do to improve the information ?