Technical FAQs

Ask a Question

Does Schneider Electric have a panel that can be used for 120/208 v 3 phase 4 wire 100 amp main breaker with bolt on branches?

Issue:
Does Schneider Electric have a panel that can be used for 120/208 v 3 phase 4 wire 100 amp main breaker with bolt on branches?

Product Line:
System Optimum Building

Environment:
Products sold and used in the United States

Cause:
Selection of correct panelboard based on voltage required

Resolution:
The NQ can be used for this requirement.

CTA-ID : 2018063

Was this helpful?
What can we do to improve the information ?