Technical FAQs

Ask a Question

What is the part number for a replacement LINE Base Assembly, LOAD Base Assy and Arc Suppressor Assembly for a H362AWK, Series E1 safety switch?

Issue:
Repair Parts

Product Line:
Obsolete HD SS

Cause:
Maintenance

Resolution:
The part numbers are:
Line base assembly - 40512-491-50,(one required)
Load base assembly - 40512-500-50 (one required)
Arc suppressor assembly - 40512-399-50 (one required)


CTA-ID : 2018048
Was this helpful?
What can we do to improve the information ?