Technical FAQs

Ask a Question

Are the busway fusible plug-in units (ex. PQ4220G) or circuit breaker plug-in units (ex. PKA36200GN) rated as a UL Service Entrance device?

None of the busway plug-in units are UL Service Entrance rated.


CTA-ID : 2017864
Was this helpful?
What can we do to improve the information ?