Technical FAQs

Ask a Question

What replaces the 8839TR01 ATV66 High Ambient Unloader since it is listed as obsolete?

The kit includes three items:  a thermistor (available only from SQD as part number 26116-78101), a 3.32kohm 1/4 watt 1% resistor (available from an electronics supply store), and the analog input control terminal from the ATV66 (J13 which can be purchased as part of kit number VZ3N006).

Crown Point has the thermistor (part number 26116-78101) or
100K ohm thermistor, Keystone Thermometrics part number RL2010-54.1K-138-D1 available by special order from Newark Electronics.

It is placed between +10V and AI2 and a 3.32K ohm 1/4W 1% metal film resistor is installed between AI2 to common.




CTA-ID : 2017674
Was this helpful?
What can we do to improve the information ?