Technical FAQs

Ask a Question

Can additional branch neutral bars be added in the field to a QO or Homeline load center?

Product Design Features

Product Line:
QO and Homeline load centers

Branch Neutral Bars


No, Square D provides up to 150% of branch neutral connections required for the number of circuits in a load center. There should not be a requirment for additional branch neutral connetions, unless the installer has used the neutral bar for equipment ground connections. In this case a separate PK ground bar should be obtain and installed in the load center to use for the equipment ground terminations.

CTA-ID : 2017503
Was this helpful?
What can we do to improve the information ?