Technical FAQs

Ask a Question

What degree of protection does the KCC1LZ handle assembly have ?

This handle is rated P65 when used with the gasket included. Also, it carries a NEMA/UL Type 1 and 12 rating.


CTA-ID : 2018039
Was this helpful?
What can we do to improve the information ?