Technical FAQs

Ask a Question

What is the maximum timing range of the Zelio-logic relay?

The maximum range goes to 99 hours, 59 minutes.
Preset value time unit. There are four possible cases:
1/100 ths. of a second: 00:00s Maximum 99.99s
1/10 th of a second: 000. 0s Maximum 999.9s
Minutes:seconds: 00:00M:S Maximum 99.59
Hours: minutes: 00:00M:S Maximum 99.59


CTA-ID : 2017844
Was this helpful?
What can we do to improve the information ?