Technical FAQs

Ask a Question

What temperatures are the 9001 Type K, Type SK, and Type KX rated for?

-22 degrees F to +140 degrees F at 50% relative humidity and -30 degrees C to +60 degrees C.


CTA-ID : 13471
Was this helpful?
What can we do to improve the information ?