Technical FAQs

Ask a Question

What is the length of the flexible cable itself for the Class 9422 Type C** flexible cable mechanisms?

The flexible cable mechanisms have a 7 inch fixed coupler on each end, therefore 14 inches must be subtracted from the published total cable length. For example, the 9422CGJ30 is published as a 36 inch cable operator, this unit has 22 inches of flexible cable.

Total 36`` - Flexible portion 22``
Total 48`` - Flexible portion 34``
Total 60`` - Flexible portion 46``
Total 120`` - Flexible portion 106``

CTA-ID : 2017313
Was this helpful?
What can we do to improve the information ?