Technical FAQs

Ask a Question

What are the dimensions and weight for the ATV31HU75N4?

This is a frame size 8 and the Width is 7.09 in (180 mm), Depth is 6.69 in (170 mm) and the height is 9.13 (232 mm).

Unit weights 10.39 lbs (4.70 kg)

This includes units: ...U55M3X ...U75M3X ...U55N4 ...U75N4 ...U55S6X ...U75S6X

CTA-ID : 2017659
Was this helpful?
What can we do to improve the information ?