Technical FAQs

Ask a Question

What is the replacement lugs for the PQ3603G Busway plug-in 30amp Switch?

Request load base assembly 45201-623-50 which contains the lugs, base, and load side fuse clips for all three phases. This applies to Series 4 plug-in units only.

CTA-ID : 2017487
Was this helpful?
What can we do to improve the information ?