Technical FAQs

Ask a Question

How do we get (3) L5-30 receptacles and (3) QO130 breakers into a plug-In unit for the Powerbus 225 busway?

You can have the factory assemble the units. Go through local field office for price and availability.

Also, you can separately purchase the QOR enclosure only from page 10-3 in the 173 Digest, purchase the QO circuit breakers, and purchase the receptacles from an outside source and install them yourself.

CTA-ID : 2017485
Was this helpful?
What can we do to improve the information ?