Technical FAQs

Ask a Question

NH1B Panelboards and Branch Circuit Breakers

Issue:
What type branch breakers are used in an obsolete NH1B panelboard? 

Product Line:
Obsolete NH1B circuit breaker panelboards that were sold and supported in the USA.

Enviroment:
Mainenance/product information 

Cause:
Selection of correct branch circuit breakers for the obsolete NH1B panelboards.

Resolution:
FY or FYB, 15-30A, 1P; FA or FAB, 15-100A, 1, 2, and 3-pole; FH or FHB 15-100A, 1,2, and 3-pole


 






CTA-ID : 2017829
Was this helpful?
What can we do to improve the information ?