Technical FAQs

Ask a Question

Where is the Powersuite configuration file located and how can it be sent to another user for use?

The configuration file is located in the User directory of the Powersuite software.
The file first has to be exported using the Export function under the File menu. This creates a file with `.ps2` extension. This file then can be emailed and the customer will then import the file using the Import function under the File menu.


CTA-ID : 2017647
Was this helpful?
What can we do to improve the information ?